Why IMX8QXP spend too much time to Initialization ldb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why IMX8QXP spend too much time to Initialization ldb

637 Views
shalanyang
Contributor II

Why IMX8QXP spend too much time to Initialization ldb ? 

should can we delete the delay time ?or decrease the time ? the code is follow:

static const struct panel_desc jdi_tx26d202vm0bwa = {
.timings = &jdi_tx26d202vm0bwa_timing,
.num_timings = 1,
.bpc = 8,
.size = {
.width = 300,
.height = 150,
},
.delay = {
/*
* The panel spec recommends one second delay
* to the below items. However, it's a bit too
* long in pratical. Based on tests, it turns
* out 100 milliseconds is fine.
*/
.prepare = 100,
.enable = 100,
.unprepare = 100,
.disable = 100,
},
.bus_format = MEDIA_BUS_FMT_ARGB8888_1X32,//MEDIA_BUS_FMT_RGB888_1X7X4_SPWG,
};

static int panel_simple_prepare(struct drm_panel *panel)
{
struct panel_simple *p = to_panel_simple(panel);
int err;
if (p->prepared)
return 0;

err = regulator_enable(p->supply);
if (err < 0) {
dev_err(panel->dev, "failed to enable supply: %d\n", err);
return err;
}
if (p->enable_gpio)
gpiod_set_value_cansleep(p->enable_gpio, 1);

printk("%s===========\n",__FUNCTION__);
if (p->desc->delay.prepare)
msleep(p->desc->delay.prepare);
printk("%s============p->desc->delay.prepare=%u\n",__FUNCTION__,p->desc->delay.prepare);
p->prepared = true;

return 0;
}

console log:

.....

[ 0.404633] panel_simple_prepare===========
[ 0.511409] panel_simple_prepare============p->desc->delay.prepare=100

.....

why delay 100ms ? can we decrease it  to 10ms or less? 

I replace msleep(p->desc->delay.prepare) with msleep(10)  ,the OS could startup normally and the 

lvds can show normal, Is there any problem ?Anyone could help me ?

0 Kudos
2 Replies

504 Views
igorpadykov
NXP Employee
NXP Employee

Hi shalan

as you noted: "The panel spec recommends one second delay.."

so seems this is panel issue, not i.MX8QXP and may be posted on

tech support jdi lcd vendor

Contact us | Japan Display Inc. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

504 Views
shalanyang
Contributor II

thanks for you answer.

you means the problem is in the lcd? different lcd may be have different spec ?so we need lcd verdor support ?

0 Kudos