工厂每次生产,都有一小部分板子跑不起来,照过X光无短路; ddr_stress_tester_v2.70 测试,能够下载初始化那端代码,但跑频率就跑不起来。分析各种情况,就觉得虚焊可能性最大。但是4片DDR和IMX6DL都是BGA封装,都用热风台吹一遍很繁琐,有没有办法定位哪一片出问题?
ddr_stress_tester 工具有个32bit Memory Read/Write功能,原以为可以读写DDR,折腾半天没找到规律,请问它是读写IMX6里的寄存器还是DDR空间?我们的4片DDR总容量1G,如果是读写DDR空间,它和DDR地址是怎么样对应的?
Hello Deng,
It is obvious that SMT process is responsible for this problem. The best way is to feedback the problem to SMT manufacturers and communicate the way of process improvement. Otherwise, it will cost a lot of manpower and material resources to repair these faulty boards in large batches.
关于这个问题,很明显是SMT工艺造成的,最好的办法是把问题反馈给SMT厂家,沟通工艺上的改进方式,否则批量大的时候,去修理这些有问题的板子,将花费很大的人力和物力。
对于已经发生的有问题的板子,不建议你自己修理,需要返厂,请他们工人在BGA工作台上进行加热处理。
Have a nice day!
NXP TIC weidong sun