AnsweredAssumed Answered

memac10 independent mode

Question asked by Mark Palamar on Dec 31, 2018
Latest reply on Jan 2, 2019 by ufedor

Is it possible to run memac10 in independent mode on the t2081 processor?  A board is configuring memac10 to use the second RGMII interface.  Memac3 is using the first RGMII interface and works fine in independent mode.  However memac10 is 1 / 2.5 / 10Gbps, so I'm wondering if it can not be used in independent mode.

 

Thanks!

Mark

Outcomes