AnsweredAssumed Answered

Capabilities YoctoProject SDK V1.8

Question asked by Sandra Trujillo García on Dec 28, 2018
Latest reply on Jan 30, 2019 by Sandra Trujillo García

I am trying to install the capabilities in my image of the yocto project with SDK V.1.8 for the T2080.
I already did it with the SDK V.2.0 for the development kit T2080RDB-PC and for them to work I had to enable the fields in the kernel:
Ext2 extended attributes
Ext2 Security Labels
In addition to saying that the 'libcap' should be installed in the .conf file. But with SDK V.1.8 I can not get the linux capabilities in my final system.

 

Searching for 'setcap' in the directory of SDK V1.8 and SDK V2.0 I have found that an executable is missing in SDK V1.8. I show this difference in the attached images. As you can see, an executable is missing in the SDK V1.8 of 'setcap' in the directory '... / rootfs / usr / sbin' I thought that maybe I did not have the capabilities with the SDK V1.8 and yes with SDK V2.0 is related to this.

 

Would someone be able to help me?

Thanks.

Outcomes