Oops: iMX6QPlus with Kernel 3.14.52

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Oops: iMX6QPlus with Kernel 3.14.52

585 Views
bakbad
Contributor III

Hello, NXP

The custom board with imx6qplus runing kernel 3.14.52 have the Oops information.Any advice?

Best Regards,

bo xu

Labels (3)
0 Kudos
1 Reply

485 Views
igorpadykov
NXP Employee
NXP Employee

Hi bo

 one can run ddr test and rebuild image with new calibration coefficients

found from test (put them in uboot/board/freescale/mx6sabresd/mx6qp.cfg)

i.MX6/7 DDR Stress Test Tool V3.00 

/external-link.jspa?url=https%3A%2F%2Fsource.codeaurora.org%2Fexternal%2Fimx%2Fuboot-imx%2Ftree%2Fbo...mx6qp.cfg\mx6sabresd\freescale\board - uboot-imx - i.MX U-Boot 

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------