Hello,
I need clarification regarding FlexSPI supported serial clock frequencies in i.MX 8X processor. As far as I could understand FlexSPI clock serialClkFreq is configured by ROM and its frequencies vary from 20 to 200 MHz.
The question is whether serialClkFreq and flexspi0_ipg_clk_sfck/flexspi1_ipg_clk_sfck is the same clock? Based on MCR0 register serial root clock can be divided maximum by 8. Does it mean that the minimum supported frequency is 2.5MHz?
Thanks,
Yuri
Hi Yuri
supported frequencies are described in i.MX8QXP Datasheet
sect.4.10.12 FlexSPI timing parameters:
The FlexSPI interface can work in SDR or DDR modes. It can operate
up to 60 MHz at 3.3 V, 166 MHz at 1.8 V SDR mode
https://www.nxp.com/docs/en/data-sheet/IMX8QXPAEC.pdf
There is no min.frequency limit, as for "2.5MHz" - one can consider
various parents clocks with dividers in Chapter 8 Clocking i.MX8DQXP Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8DQXPRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------