Difference between samples with MTRCKTSBNZVM128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between samples with MTRCKTSBNZVM128

377 Views
hiro2hiro
Contributor I

Hi,

I am trying motor control with MTRCKTSBNZVM128.

I want someone to answer my question.

I am using the samples MTRCKTSBNZVM128_HALL_CW11 and MTRCKTSBNZVM128_SENSORLESS_CW10.

As shown in the graph below, HALL (1) has larger current consumption than SENSORLESS.

The horizontal axis is the number of revolutions [rpm], and the vertical axis is the current [A].

pastedImage_1.png

However, when you try at a certain time, it is equivalent to SENSORLESS like HALL (2).

I confirmed the source code, but I think both are 120 degree conduction, not vector control.

I have not changed the NXP kit at all.

Is there a possibility that the HALL sample behaves like SENSORLESS under some conditions?

I'd like to receive advice.

Thank you.

0 Kudos
0 Replies