Two Questions on Running Qt5 webengine on i.mx6q Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two Questions on Running Qt5 webengine on i.mx6q Linux

1,711 Views
poorstudio
Contributor I

Two Questions on Running Qt5 webengine on i.mx6q Linux

The following is running chromium-browser. webgl  is ok

pastedImage_1.png

But there are two problems under Qt5 webengine:

1. The following is running qt-everywhere-src-5.11.2/qtwebengine/examples/webengine/minimal. webgl is ng

pastedImage_2.png

    but  qt-everywhere-src-5.11.2/qt3d/examples/qt3d/lights 3d is ok.

    pastedImage_3.png

    2. qt-everywhere-src-5.11.2/qtwebengine/examples/webenginewidgets/simplebrowser
     not show web. Display black screen.
     pastedImage_4.png
0 Kudos
4 Replies

1,160 Views
igorpadykov
NXP Employee
NXP Employee

Hi tom

as described in sect.5.6.6 Chromium Browser attached Yocto Guide:

"The Yocto Project community has chromium-imx recipes..Note that NXP does

not support or test the patches from the community, neither for VPU or GPU support."

In general issue also may be posted on  meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,160 Views
poorstudio
Contributor I

I forgot to display the results of html5test.com. Show support webgl

pastedImage_1.png

pastedImage_2.png

0 Kudos

1,160 Views
poorstudio
Contributor I

in qt-everywhere-src-5.11.2/qtwebengine/examples/webenginewidgets/simplebrowser. It's lsame as in qt-everywhere-src-5.11.2/qtwebengine/examples/webengine/minimal

pastedImage_1.png

pastedImage_2.png

0 Kudos

1,160 Views
poorstudio
Contributor I

In second question,browser display page part is black screen

0 Kudos