AnsweredAssumed Answered

Recommended decoupling RT1064?

Question asked by Carsten Groen on Dec 16, 2018
Latest reply on Dec 16, 2018 by Carsten Groen

In the RT1050/RT1060 Hardware Development Guide: https://www.nxp.com/docs/en/user-guide/MIMXRT105060HDUG.pdf 

on page 3 is a list of the various power connections and the recommended decoupling capacitors. For Pin VDD_SNVS_CAP is listed 1 x 0.22uF and 1 x 4.7uF:

 

 

On the other hand, when looking at the EVK schematics for the 1064EVK, only a single 0.22uF capactor is shown:

 

 

Which one is "the most recommended" way ?

 

 

Also, the NVCC_PLL signal is not mentioned in the Hardware Development Guide, according to the EVK, there is a single 0.22uF and a single 4.7uF as decoupling, I assume this is the recommended way ?

Outcomes