Hi professors,
I found the KL03z have a slider pad so I think it should be used,but maybe it`s not like KL25z has a Tsi pin for ,and that I am trying to build a TSI function for KL03z then it couldn`t work, Is it a GPIO or the other pins for use?
Then I found a TSS Library can be built for extension development board,but I tried to build with Codewarrior and I failed.Is there anyway can try for it?
Thanks for Helping!
Hi Hans,
KL03 hasn't TSI module. It use GPIO and external circuit to charge and discharge touch electrode.
The TSS_3_1 library support CW. It has KL02 demo. And KL03 and KL02 are almost same.
Regards,
Jing
Hi Jing,
It`s really thanks for your help!
And,can I ask about KL02 function that I tried to connect to KL03 board?
Is there need some settings for KL03Z? I configured the KL03 pin defined and the other. Then I started to Debug,but It came out an error like down below.
Is there something I missed? and can you help me to figure out?
Really appreciate,
Hans