I want to operate mcu KL4x on a lower frequency than the normal 48MHz. Is it possible ?
Hi Kostas Nomikos
Yes, it is possible. Are you using KL43 or KL46? These two devices have different clock module (MCG and MCG-lite). I recommend you the following link:
https://www.nxp.com/files-static/training_pdf/28973_S08_MCG_WBT.pdf
It is for MCG and it explains in detail the different clock modes. Actually, out of reset, Kinetis devices work in FEI mode which doesn't run to the 48MHz.
I highly recommend you SDK software tools, You can download it from
It includes a clock config tool where you can set the frequency that needs.
Hope this information could help you, please don't hesitate to contact me if you have any other question about this.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I am using KL46Z. Thanks for your help, much appreciated.
Kostas
There are various clocking options:
See some references for the KL46 at
http://www.utasker.com/kinetis/FRDM-KL46Z.html
http://www.utasker.com/kinetis/TWR-KL46Z48M.html
including simulation of the operation and clock settings.
Regards
Mark