AnsweredAssumed Answered

RT1060/1064 Ethernet w/SEMC Pin Config

Question asked by Heath Pritchett on Dec 11, 2018
Latest reply on Dec 20, 2018 by Heath Pritchett

Hi,

 

I am currently using the RT1050 and have configured the Ethernet, LCD, and SDRAM(using the SEMC). I am wanting to know if I can migrate to the RT1060/1064 and gain a second Ethernet port. Using the pinmux tool it will allow me to select the second Ethernet port but the pins are shared with either the SEMC or the LCD pins. The pinmux tool does not show any conflict when both are selected. So my question is: can I use the ethernet and SEMC at the same time? Or is there some other way I can configure this to work to use all of the above?

 

Thanks in advance!

Outcomes