Thank you for your help.
MKM14Z64ACHH5 is carried in the product to be shipped.
The question is below.
① Is there something wrong with using LPC-LINK2 to write and ship with the CMSIS-DAP interface? (Are there any conditions such as unavailability for mass production?
② If there is a problem, is there any writer recommended by NXP?
Thank you.
I am sorry that my English is not fine.
Solved! Go to Solution.
Thank you for answering.
There are license terms on the following pages.
https://www.segger.com/products/debug-probes/j-link/models/other-j-links/lpc-link-2/
->The firmware may only be used for development and/or evaluation purposes. It may not be used for production purposes.
According to this, it seems that it can not be used for products for evaluation.
OK. Thank you very much.
Hi jun yamada,
① Is there something wrong with using LPC-LINK2 to write and ship with the CMSIS-DAP interface? (Are there any conditions such as unavailability for mass production?
Answer: You can use the LPC-LINK2 to program your MKM14Z64CHH5, but I suggest you use the LPC-LINK2 with the JLINK firmware.
You can use the LPCScrypt to change the LPC-LINK2 firmware, which can be download from this link:
② If there is a problem, is there any writer recommended by NXP?
Answer: LPC-LINK2 with JLINK can debug your chip, it's no problem.
About the other programmer or debugger, you can use: Segger JLINK, P&E Multilink, both these debugger can be used on your side.
Wish it helps you!
If you still have question about it, please kindly let me know.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for answering.
There are license terms on the following pages.
https://www.segger.com/products/debug-probes/j-link/models/other-j-links/lpc-link-2/
->The firmware may only be used for development and/or evaluation purposes. It may not be used for production purposes.
According to this, it seems that it can not be used for products for evaluation.
OK. Thank you very much.
OK, then if in the mass production, it's better to use the specific debugger, like SEGGER JLINK ,P&E multilink.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------