READ WRONG DEVICE ID IN DIFFERENT BOARD BUT SAME SBC UJA1075ATW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

READ WRONG DEVICE ID IN DIFFERENT BOARD BUT SAME SBC UJA1075ATW

Jump to solution
1,882 Views
alighieri
Contributor III

WE CURRENTLY ARE WORKING DOWN FOR OUR EMERGENT CASE WHICH IS ASKED BY END CUSTOMER FOR EXPECTED DATE OF MASS PRODUCTION ON 28 FEB 2019. THE PROBLEM IS ADOPTED SBC UJA1075ATW WITH READING BACK UNKNOWN DEVICE ID.

ACCORDING TO A LIST OF DEVICE IDS IN APPLICATION NOTE AH1002 THE ID SHOULD BE

UJA0175A 0X5208

UJA1076A 0X5008

UAJ1078A 0X5308

UAJ1079A 0X5200

IN THE CASE WE USE THE HOST MCU S32K116 ALONG WITH SBC UJA1075ATW

BUT WHAT WE READ BACK IS

0x5002

 

IN THE OTHER BOARD DESIGNED WITH SAME SBC UJA1075ATW BUT DIFFERENT HOST MCU KINETIS EA

WHAT WE READ BACK

0x5004

WHATEVER WE TRY THE OTHER BOARD IN SAME MCU AND SBC

THEY ALWAYS READ WRONG DEVICE IDS

IN KINETIS EA 128 + SBC UJA1075ATW 0x5004

IN S32K116 + SBC UJA1075ATW 0x5002

IT'S STRANGE SINCE THE DEVICE ID ISN'T LISTED IN AH1002 AT ALL.

AND WE CANNOT WRITE TO CONTROL THE SBC UJA1075ATW.

WHAT REASON WILL CAUSE A DIFFERENT DEVICE ID READ BACK BY DIFFERENT MCU IN SAME SBC?

CAN YOU HELP TO FIND OUT WHAT THE PROBLEM IS?

AND HERE IS DOESN'T A CHIP PART NUMBER MATCHED WITH WHAT WE USE

UJA1075ATW

BUT

pastedImage_19.png

DATASHEET IS NO DOUBT RIGHT BUT IN APPLICATION NOTE AH1002 WE FIND NO UAJ1075ATW LISTED HERE.  AND WE HAVE DEFINITELY CONFIRMED FOLLOWING IO

1. WD OFF - ACTIVE HIGH TO DISABLE

2. CHIP SELECT - ACTIVE LOW TO ENABLE

PLEASE SEE FOLLOWING SCREENSHOTS OF SCHEMATIC

pastedImage_1.png

pastedImage_19.png

2-1. AS YOU SEE THE HARDWARE DESIGN IS DIFFERENT FROM YOUR PROVIDED DESIGN REFERENCE ESPECIALLY:

pastedImage_2.png

IF THE HOST MCU IS NOT READY AND CONFIGURE THE IO ACTIVE HIGH THEN WDOFF WILL BE ACTIVE IN OUR DESIGN. WE THINK IT A BIG MISTAKE DUE TO OUR CASE REQUIRED TO UPDATE CODES BY CAN FLASH BOOTLOADER.

2-2. ANOTHER BIG PROBLEM WITH OUR DESIGN AS YOU SEE IS THE 2 SETS OF PINNING WAKEUP. 

I DON'T HAVE IDEAS ABOUT THE ERROR DEVICE ID. IS IT POSSIBLE CAUSED BY HARDWARE DESIGN MISSES?

AND HERE ARE 2 KIND OF SAMPLE CODES PROVIDED BY YOU:

UJA107XA CODE.ZIP

LOOKS A SAMPLE CODES FOR S12X SERIES CHIPSET AND CANNOT BE APPLIED DIRECTLY IN LATEST S32K11X AND KINETIS EA.

pastedImage_26.png

UJA107XA CODE RAR

WITH MORE SIMPLE SAMPLE CODES WHICH ARE NOT SPECIFIC FOR A CHIPSET AND MATCH THE APPLICATION HINT

pastedImage_25.png

WHAT IS THE DEFINITE ONE?

CAN YOU PROVIDE SAMPLE CODES FOR

S32K116

KINETIS EA

WE HAVE VERY URGENT CASE READY FOR MASS PRODUCTION IN SCHEDULED DATE 28 FEB 2019.

---------------------------------------------------------------------------------------------------------------------------------------------------------------

WE'VE FOUND OUT ANOTHER ISSUE WITH INT PIN. THE INT PIN KEEPS IN SEEDING INTERRUPT TO MCU WHEN POWER ON. DOES IT THE FACTOR CAUSE WE READ BACK WRONG DEVICE IDS? FROM YOUR DATASHEET HERE ARE LOTS OF REASONS THE INT PIN WILL SEND INTERRUPT TO HOST MCU AS BELOW:

pastedImage_1.png

pastedImage_2.png

SEEMS IF V1 / V2 UNDERVOLTAGE OR DESIGN MISSES WILL CAUSE INTERRUPT OUT TO HOST MCU?

0 Kudos
1 Solution
1,655 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Your issue has solved because of the wrong SPI timing.

View solution in original post

0 Kudos
1 Reply
1,656 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Your issue has solved because of the wrong SPI timing.

0 Kudos