AnsweredAssumed Answered

which pin is "gpio_3" for low power boot mode?

Question asked by David Luberger on Dec 7, 2018
Latest reply on Dec 12, 2018 by gusarambula

The SoloX reference manual says when fuses are set to enable Low Power Boot mode, it looks to a GPIO pin called "GPIO_3" to determine whether it should boot into low power mode. However, there is no pad called "GPIO_3".  All GPIOs have the naming convention "GPIOx_IOyy" where x is the GPIO group number and yy is a number from 00 to 31.  So what pin is the low power mode input referring to?

Outcomes