imx6solox audio volue addition and subtraction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6solox audio volue addition and subtraction

964 Views
1773750986
Contributor I

I  want  to  add  two Volume addition and subtraction buttons,should i  add  this  two GPIO to 1.8V  CSI module which control  WM8962BECSN/R   or  other Casual 3.3V  module?button1.pngbutton2.png

button3.png

Labels (1)
Tags (1)
0 Kudos
4 Replies

872 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

for volume control examples one can check sect.28.5.1 Stereo Codec Unit Test

attached Linux Manual and unit test package ( ../mxc_sound_test)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

872 Views
1773750986
Contributor I

You misunderstood what I meant. I didn't want to ask you about the software. What I want to ask is about the hardware ,where do I connect  the Volume adjustment button. Is 1.8V gpio or the 3.3V GPIO?

0 Kudos

872 Views
igorpadykov
NXP Employee
NXP Employee

you can use any gpio for such purpose, ir does not not matter "1.8V gpio or the 3.3V GPIO".

0 Kudos

872 Views
1773750986
Contributor I

ok ,thanks very  much!

0 Kudos