Hi All,
Recently I migrated from CW 10.6 to KDS 3.2.
I have ported application successfully.
I have some query regarding bootloader
1) Can i use CW bootloader? (I am converting .S19 which is generated by CW to .bin file using "Burner" software)
2) If not than Please help me to generate bootloader file.
Regards,
Mayur
Hi Mayur Savaj,
Of course, you can use the CW bootloader, both the CW bootloader and the KDS bootloader you can use.
If you CW bootloader, you can use the CW associated with the debugger to download the bootloader code to the chip.
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------