Where can I download the microcode for the 8270?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I download the microcode for the 8270?

Jump to solution
814 Views
pdeiber
Contributor I

I need to apply the patch for addressing Ethernet issues on 8270. Is there an official link for this patch/microcode?

Thx,

Patrick

Labels (1)
Tags (2)
1 Solution
659 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

It seems there is no an official link for this patch/microcode. At least I could not find it. I recommend creating technical case (see https://community.nxp.com/thread/381898) with request for CPM111+CPM118+CPM119 microcode patch. I know you can get it in this way.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
660 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

It seems there is no an official link for this patch/microcode. At least I could not find it. I recommend creating technical case (see https://community.nxp.com/thread/381898) with request for CPM111+CPM118+CPM119 microcode patch. I know you can get it in this way.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------