Radio tuner Si4741 configuration in imx6dl-sabresd.dts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Radio tuner Si4741 configuration in imx6dl-sabresd.dts

358 Views
avinashtiwaskar
Contributor I

How to enable Radio tuner Si4741 in device tree (imx6dl-sabresd.dts) on iMX6 custom board? I am looking for the sample device tree which I can use to setup the radio tuner. Radio tuner is connected over I2C. Below is the snapshot of the changes made:

pinctrl_si4741: si4741-grp {
// Need to update clock....(MX6QDL_PAD_GPIO_8__SPDIF_SR_CLK).?
// MX6QDL_PAD_GPIO_8__GPIO1_IO08 0xxxxx
// 2 Wire operation (I2C): GPIO1 1 (3.3V), GPIO2 0
// Verify how to set GPIO2 to 0..
// fsl,pins = <MX6QDL_PAD_EIM_D20__GPIO3_IO20 0x00000000>;
fsl,pins = <MX6QDL_PAD_EIM_D16__GPIO3_IO16 0x0f0b0 /* RADIO_RST */
MX6QDL_PAD_EIM_D17__GPIO3_IO17 0x0f0b0 /* RADIO_SEN_N - p2193 */
MX6QDL_PAD_EIM_D20__GPIO3_IO20 0x0f0b0 /* RADIO_GPIO2/INT_N - PULL Down Rst - p2199 */
MX6QDL_PAD_EIM_D21__GPIO3_IO21 0x80000000 /* RADIO_GPIO3/DCLK p2201*/
MX6QDL_PAD_GPIO_8__GPIO1_IO08 0x80000000 /* 0x10011 - CLK_RADIO_RCLK - 32768 Max 40000 KHz : p2477 */
>;
};

pinctrl_i2c2: i2c2grp {
// MX6QDL_PAD_KEY_COL3__I2C2_SCL -- MX6QDL_PAD_KEY_ROW3__I2C2_SDA
fsl,pins = <0x250 0x638 0x870 0x4 0x1 0x4001b8b1 0x264 0x64c 0x874 0x4 0x1 0x4001b8b1>;
};

i2c2: i2c@021a4000 {
   #address-cells = <0x1>;
   #size-cells = <0x0>;
   compatible = "fsl,imx6q-i2c", "fsl,imx21-i2c";
   reg = <0x21a4000 0x4000>;
   interrupts = <0 37 IRQ_TYPE_LEVEL_HIGH>;
   clocks = <&clks IMX6QDL_CLK_I2C2>;
   status = "okay";
   clock-frequency = <0x186a0>;
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_i2c2>;

      radio-si4741@11 {
      compatible = "silabs,si4741";
      reg = <0x11>;
      // vio-supply = <&si4741_vio>;
      // vdd-supply = <&si4741_vd>;
      // vddio-supply = <&reg3p3v>;
      // revision-a10; // set to default A10 compatible command set
      // MX6QDL_PAD_EIM_D20__GPIO3_IO20 /* RADIO_GPIO2/INT_N */
      // MX6QDL_PAD_EIM_D16__GPIO3_IO16 /* RADIO_RST */
      interrupts-extended = <&gpio3 20 IRQ_TYPE_EDGE_FALLING>; /* */
      reset-gpios = <&gpio3 16 GPIO_ACTIVE_HIGH>; /* RST - Active Low */
      pinctrl-0 = <&pinctrl_si4741>;
      };

};

I'm not sure if there is any other entry to be made to enable it. Or am I missing any parameter for any of the nodes mentioned above.

If someone can provide the sample .dts file which has configuration for any radio tuner, that would help.

Thanks,

Avi

0 Kudos
0 Replies