In the sample code "lpcxpresso51u68_COM_cmsis_spi_interrupt_transfer"
On the board only shows D0,D1,D2...D15, they should be match for Arduino Uno
There is no pin# definition about J1 and J2 on the guideline of the dev board, so how can I figure out which pin is J1 pin 11, pin 13, pin 15 and J2 pin 8
Hi,
You can find more information in the user manual for this board.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sol,
Thanks for your reply, but the manual did not include the pin definition.
I can't even find the first pin of J1#1 in the manual, now I can just trace the pin 1by1.