AnsweredAssumed Answered

How do I get my KITPF0100EPEVBE board connected to my KITPFGUI 4.0 graphical user interface

Question asked by Kerry Anyanwu on Nov 27, 2018
Latest reply on Nov 28, 2018 by Kerry Anyanwu

So I followed the step by step instructions on powering up the PMIC KITPF0100EPEVBE board. I connected the PF programmer (KITPFPGMEVME)  to the board via the 8-conductor flat ribbon cable and the USB to my computer (FYI, I tried this for my windows 7 and 10 machines). The USB was detected and the driver installed. I then proceeded to install the KITPFGUI software. The software installed correctly and the log showed that the device was found.device found

I tried clicking on the other tabs but they wouldn't open. when I clicked on "Scan For Devices" button I would get the error "Object reference not set to an instance of an object." And I would click ok about 6 times for the error to clear.

Clicking on the "Scan For Devices" button

I then proceeded to click on the Enable Target checkbox and I got the error "No Target Detected!"

Clicking on the "Enable Target" Checkbox

Here is a picture of my hardware connected via the PF-programmer

Connected via PF-programmer

and I also connected it directly via the mini USB port. I was able to read some voltages.

Connected via mini USB

Please, any assistance will be greatly appreciated. For now, this is a show stopper for me. Thanks.

Outcomes