Adding BlueZ to Yocto Build for iMx8QM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding BlueZ to Yocto Build for iMx8QM

1,110 Views
ratnakar_vibhu1
Contributor II

Hi All,

Currently we are using the iMx8QM EVK with yocto linux running on it.

My query is regarding how to enable the blueZ utility in the same. I added DISTRO_FEATURES_append += "bluez5" in local .conf file but while bitbake command there are compilation error regarding the gstreamer as below-

 ../../../../git/gst-libs/gst/app/gstappsrc.c: In function 'gst_app_src_class_init':
| ../../../../git/gst-libs/gst/app/gstappsrc.c:290:37: error: 'GST_TYPE_APP_STREAM_TYPE' undeclared (first use in this function)
|            "the type of the stream", GST_TYPE_APP_STREAM_TYPE,
|                                      ^~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/app/gstappsrc.c:290:37: note: each undeclared identifier is reported only once for each function it appears in
| ../../../../git/gst-libs/gst/video/navigation.c: In function 'gst_query_list_add_command':
| ../../../../git/gst-libs/gst/video/navigation.c:238:24: error: 'GST_TYPE_NAVIGATION_COMMAND' undeclared (first use in this function)
|    g_value_init (&item, GST_TYPE_NAVIGATION_COMMAND);
|                         ^~~~~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/navigation.c:238:24: note: each undeclared identifier is reported only once for each function it appears in
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'compute_matrix_to_RGB':
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: error: 'GST_TYPE_VIDEO_MATRIX_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
|                                           ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
|  #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
|                                ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1406:32: note: in expansion of macro 'CHECK_MATRIX_NONE'
|    if (!convert->unpack_rgb && !CHECK_MATRIX_NONE (convert)) {
|                                 ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: note: each undeclared identifier is reported only once for each function it appears in
|      GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
|                                           ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
|  #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
|                                ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1406:32: note: in expansion of macro 'CHECK_MATRIX_NONE'
|    if (!convert->unpack_rgb && !CHECK_MATRIX_NONE (convert)) {
|                                 ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'compute_matrix_to_YUV':
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: error: 'GST_TYPE_VIDEO_MATRIX_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
|                                           ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
|  #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
|                                ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1424:40: note: in expansion of macro 'CHECK_MATRIX_NONE'
|    if (force || (!convert->pack_rgb && !CHECK_MATRIX_NONE (convert))) {
|                                         ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_convert_to_RGB':
| ../../../../git/gst-libs/gst/video/video-converter.c:822:41: error: 'GST_TYPE_VIDEO_GAMMA_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_GAMMA_MODE, GST_TYPE_VIDEO_GAMMA_MODE, DEFAULT_OPT_GAMMA_MODE)
|                                          ^
| ../../../../git/gst-libs/gst/video/video-converter.c:851:31: note: in expansion of macro 'GET_OPT_GAMMA_MODE'
|  #define CHECK_GAMMA_REMAP(c) (GET_OPT_GAMMA_MODE(c) == GST_VIDEO_GAMMA_MODE_REMAP)
|                                ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1575:14: note: in expansion of macro 'CHECK_GAMMA_REMAP'
|    do_gamma = CHECK_GAMMA_REMAP (convert);
|               ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_hscale':
| ../../../../git/gst-libs/gst/video/video-converter.c:828:47: error: 'GST_TYPE_VIDEO_RESAMPLER_METHOD' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_RESAMPLER_METHOD, GST_TYPE_VIDEO_RESAMPLER_METHOD, \
|                                                ^
| ../../../../git/gst-libs/gst/video/video-converter.c:1618:12: note: in expansion of macro 'GET_OPT_RESAMPLER_METHOD'
|    method = GET_OPT_RESAMPLER_METHOD (convert);
|             ^~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_vscale':
| ../../../../git/gst-libs/gst/video/video-converter.c:828:47: error: 'GST_TYPE_VIDEO_RESAMPLER_METHOD' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_RESAMPLER_METHOD, GST_TYPE_VIDEO_RESAMPLER_METHOD, \
|                                                ^
| ../../../../git/gst-libs/gst/video/video-converter.c:1650:12: note: in expansion of macro 'GET_OPT_RESAMPLER_METHOD'
|    method = GET_OPT_RESAMPLER_METHOD (convert);
|             ^~~~~~~~~~~~~~~~~~~~~~~~
| Makefile:873: recipe for target 'libgstvideo_1.0_la-navigation.lo' failed
| make[5]: *** [libgstvideo_1.0_la-navigation.lo] Error 1
| make[5]: *** Waiting for unfinished jobs....
| ../../../../git/gst-libs/gst/tag/tags.c: In function 'gst_tag_image_type_is_valid':
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_convert':
| ../../../../git/gst-libs/gst/tag/tags.c:235:29: warning: implicit declaration of function 'gst_tag_image_type_get_type' [-Wimplicit-function-declaration]
|    klass = g_type_class_ref (gst_tag_image_type_get_type ());
|                              ^~~~~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/tags.c:235:3: warning: nested extern declaration of 'gst_tag_image_type_get_type' [-Wnested-externs]
|    klass = g_type_class_ref (gst_tag_image_type_get_type ());
|    ^~~~~
| Makefile:673: recipe for target 'libgstapp_1.0_la-gstappsrc.lo' failed
| make[5]: *** [libgstapp_1.0_la-gstappsrc.lo] Error 1
| make[5]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/app'
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: error: 'GST_TYPE_VIDEO_MATRIX_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
|                                           ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
|  #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
|                                ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1727:7: note: in expansion of macro 'CHECK_MATRIX_NONE'
|    if (CHECK_MATRIX_NONE (convert)) {
|        ^~~~~~~~~~~~~~~~~
| Makefile:561: recipe for target 'all' failed
| make[4]: *** [all] Error 2
| make[4]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/app'
| ../../../../git/gst-libs/gst/video/video-converter.c:824:45: error: 'GST_TYPE_VIDEO_PRIMARIES_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_PRIMARIES_MODE, GST_TYPE_VIDEO_PRIMARIES_MODE, DEFAULT_OPT_PRIMARIES_MODE)
|                                              ^
| ../../../../git/gst-libs/gst/video/video-converter.c:853:34: note: in expansion of macro 'GET_OPT_PRIMARIES_MODE'
|  #define CHECK_PRIMARIES_NONE(c) (GET_OPT_PRIMARIES_MODE(c) == GST_VIDEO_PRIMARIES_MODE_NONE)
|                                   ^~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1735:7: note: in expansion of macro 'CHECK_PRIMARIES_NONE'
|    if (CHECK_PRIMARIES_NONE (convert)) {
|        ^~~~~~~~~~~~~~~~~~~~
| Makefile:837: recipe for target 'app' failed
| make[3]: *** [app] Error 2
| make[3]: *** Waiting for unfinished jobs....
| ../../../../git/gst-libs/gst/video/video-converter.c:822:41: error: 'GST_TYPE_VIDEO_GAMMA_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_GAMMA_MODE, GST_TYPE_VIDEO_GAMMA_MODE, DEFAULT_OPT_GAMMA_MODE)
|                                          ^
| ../../../../git/gst-libs/gst/video/video-converter.c:851:31: note: in expansion of macro 'GET_OPT_GAMMA_MODE'
|  #define CHECK_GAMMA_REMAP(c) (GET_OPT_GAMMA_MODE(c) == GST_VIDEO_GAMMA_MODE_REMAP)
|                                ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1779:14: note: in expansion of macro 'CHECK_GAMMA_REMAP'
|    do_gamma = CHECK_GAMMA_REMAP (convert);
|               ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/tags.c: In function 'gst_tag_image_data_to_image_sample':
| ../../../../git/gst-libs/gst/tag/tags.c:562:23: error: 'GST_TYPE_TAG_IMAGE_TYPE' undeclared (first use in this function)
|          "image-type", GST_TYPE_TAG_IMAGE_TYPE, image_type, NULL);
|                        ^~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/tags.c:562:23: note: each undeclared identifier is reported only once for each function it appears in
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_convert_to_YUV':
| ../../../../git/gst-libs/gst/video/video-converter.c:822:41: error: 'GST_TYPE_VIDEO_GAMMA_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_GAMMA_MODE, GST_TYPE_VIDEO_GAMMA_MODE, DEFAULT_OPT_GAMMA_MODE)
|                                          ^
| ../../../../git/gst-libs/gst/video/video-converter.c:851:31: note: in expansion of macro 'GET_OPT_GAMMA_MODE'
|  #define CHECK_GAMMA_REMAP(c) (GET_OPT_GAMMA_MODE(c) == GST_VIDEO_GAMMA_MODE_REMAP)
|                                ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1935:14: note: in expansion of macro 'CHECK_GAMMA_REMAP'
|    do_gamma = CHECK_GAMMA_REMAP (convert);
|               ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_dither':
| ../../../../git/gst-libs/gst/video/video-converter.c:836:44: error: 'GST_TYPE_VIDEO_DITHER_METHOD' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_DITHER_METHOD, GST_TYPE_VIDEO_DITHER_METHOD, \
|                                             ^
| ../../../../git/gst-libs/gst/video/video-converter.c:1996:12: note: in expansion of macro 'GET_OPT_DITHER_METHOD'
|    method = GET_OPT_DITHER_METHOD (convert);
|             ^~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'convert_get_alpha_mode':
| ../../../../git/gst-libs/gst/video/video-converter.c:816:41: error: 'GST_TYPE_VIDEO_ALPHA_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_ALPHA_MODE, GST_TYPE_VIDEO_ALPHA_MODE, DEFAULT_OPT_ALPHA_MODE)
|                                          ^
| ../../../../git/gst-libs/gst/video/video-converter.c:841:30: note: in expansion of macro 'GET_OPT_ALPHA_MODE'
|  #define CHECK_ALPHA_COPY(c) (GET_OPT_ALPHA_MODE(c) == GST_VIDEO_ALPHA_MODE_COPY)
|                               ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:2222:9: note: in expansion of macro 'CHECK_ALPHA_COPY'
|      if (CHECK_ALPHA_COPY (convert))
|          ^~~~~~~~~~~~~~~~
| Makefile:811: recipe for target 'libgsttag_1.0_la-tags.lo' failed
| make[5]: *** [libgsttag_1.0_la-tags.lo] Error 1
| make[5]: *** Waiting for unfinished jobs....
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'video_converter_compute_resample':
| ../../../../git/gst-libs/gst/video/video-converter.c:826:42: error: 'GST_TYPE_VIDEO_CHROMA_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_CHROMA_MODE, GST_TYPE_VIDEO_CHROMA_MODE, DEFAULT_OPT_CHROMA_MODE)
|                                           ^
| ../../../../git/gst-libs/gst/video/video-converter.c:860:31: note: in expansion of macro 'GET_OPT_CHROMA_MODE'
|  #define CHECK_CHROMA_NONE(c) (GET_OPT_CHROMA_MODE(c) == GST_VIDEO_CHROMA_MODE_NONE)
|                                ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:2664:7: note: in expansion of macro 'CHECK_CHROMA_NONE'
|    if (CHECK_CHROMA_NONE (convert))
|        ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/gstvorbistag.c: In function 'gst_tag_to_metadata_block_picture':
| ../../../../git/gst-libs/gst/tag/gstvorbistag.c:572:49: error: 'GST_TYPE_TAG_IMAGE_TYPE' undeclared (first use in this function)
|    gst_structure_get (mime_struct, "image-type", GST_TYPE_TAG_IMAGE_TYPE,
|                                                  ^~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/gstvorbistag.c:572:49: note: each undeclared identifier is reported only once for each function it appears in
| Makefile:769: recipe for target 'libgsttag_1.0_la-gstvorbistag.lo' failed
| make[5]: *** [libgsttag_1.0_la-gstvorbistag.lo] Error 1
| make[5]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/tag'
| Makefile:636: recipe for target 'all' failed
| make[4]: *** [all] Error 2
| make[4]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/tag'
| Makefile:837: recipe for target 'tag' failed
| make[3]: *** [tag] Error 2
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'get_scale_format':
| ../../../../git/gst-libs/gst/video/video-converter.c:5794:3: warning: enumeration value 'GST_VIDEO_FORMAT_NV12_10LE' not handled in switch [-Wswitch]
|    switch (format) {
|    ^~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'setup_scale':
| ../../../../git/gst-libs/gst/video/video-converter.c:828:47: error: 'GST_TYPE_VIDEO_RESAMPLER_METHOD' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_RESAMPLER_METHOD, GST_TYPE_VIDEO_RESAMPLER_METHOD, \
|                                                ^
| ../../../../git/gst-libs/gst/video/video-converter.c:5923:12: note: in expansion of macro 'GET_OPT_RESAMPLER_METHOD'
|    method = GET_OPT_RESAMPLER_METHOD (convert);
|             ^~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'video_converter_lookup_fastpath':
| ../../../../git/gst-libs/gst/video/video-converter.c:822:41: error: 'GST_TYPE_VIDEO_GAMMA_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_GAMMA_MODE, GST_TYPE_VIDEO_GAMMA_MODE, DEFAULT_OPT_GAMMA_MODE)
|                                          ^
| ../../../../git/gst-libs/gst/video/video-converter.c:851:31: note: in expansion of macro 'GET_OPT_GAMMA_MODE'
|  #define CHECK_GAMMA_REMAP(c) (GET_OPT_GAMMA_MODE(c) == GST_VIDEO_GAMMA_MODE_REMAP)
|                                ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:6650:7: note: in expansion of macro 'CHECK_GAMMA_REMAP'
|    if (CHECK_GAMMA_REMAP (convert) && (!same_size || in_transf != out_transf))
|        ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: error: 'GST_TYPE_VIDEO_MATRIX_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
|                                           ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
|  #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
|                                ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:6661:7: note: in expansion of macro 'CHECK_MATRIX_NONE'
|    if (CHECK_MATRIX_NONE (convert)) {
|        ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:824:45: error: 'GST_TYPE_VIDEO_PRIMARIES_MODE' undeclared (first use in this function)
|      GST_VIDEO_CONVERTER_OPT_PRIMARIES_MODE, GST_TYPE_VIDEO_PRIMARIES_MODE, DEFAULT_OPT_PRIMARIES_MODE)
|                                              ^
| ../../../../git/gst-libs/gst/video/video-converter.c:853:34: note: in expansion of macro 'GET_OPT_PRIMARIES_MODE'
|  #define CHECK_PRIMARIES_NONE(c) (GET_OPT_PRIMARIES_MODE(c) == GST_VIDEO_PRIMARIES_MODE_NONE)
|                                   ^~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:6671:7: note: in expansion of macro 'CHECK_PRIMARIES_NONE'
|    if (CHECK_PRIMARIES_NONE (convert)) {
|        ^~~~~~~~~~~~~~~~~~~~
| Makefile:915: recipe for target 'libgstvideo_1.0_la-video-converter.lo' failed
| make[5]: *** [libgstvideo_1.0_la-video-converter.lo] Error 1
| make[5]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/video'
| Makefile:715: recipe for target 'all' failed
| make[4]: *** [all] Error 2
| make[4]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/video'
| ERROR: oe_runmake failed
| Makefile:837: recipe for target 'video' failed
| make[3]: *** [video] Error 2
| make[3]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst'
| Makefile:534: recipe for target 'all-recursive' failed
| make[2]: *** [all-recursive] Error 1
| make[2]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs'
| Makefile:673: recipe for target 'all-recursive' failed
| make[1]: *** [all-recursive] Error 1
| make[1]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build'
| Makefile:604: recipe for target 'all' failed
| make: *** [all] Error 2
| ERROR: Function failed: do_compile (log file is located at /home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/temp/log.do_compile.22664)
ERROR: Task (/home/airbus/iwg27-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.12.2.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3220 tasks of which 3219 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  /home/airbus/iwg27-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.12.2.bb:do_compile
Summary: There were 3 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

Request you all to please suggest, how can I solve this issue or any other way to add blueZ utility to yocto linux.

Thanks & Regards,

Ratnakar

1 Reply

826 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot help you with that, since the i.MX8QM is not officialy released yet and we do not have a way to test your problem. I apologize for the inconveniences this could give you.

Best Regards,

Diego