I am trying to use MPC574XG_MCAL4_0_RTM_1_0_5 along with tresos, when I try to load configuration for it the following error is seen:
[Project: Calypso6M_MCAL4_0_sample_ap Plug-in with a module "Dem_TS_T2D35M10I3R0" is not installed - cannot create module configurations for project "Calypso6M_MCAL4_0_sample_ap"].
I think this error should not be there in the first place as all the plugins installer are of type xx_yy_abcd10I5R0, because i am using _1_0_5 version and not the _1_0_3.
I searched google for relevant problems but did not find any answer. Any help will be appreciated.
Thank you.
Hi,
[Project: Calypso6M_MCAL4_0_sample_ap Plug-in with a module "Dem_TS_T2D35M10I3R0" is not installed - cannot create module configurations for project "Calypso6M_MCAL4_0_sample_ap"].
Is the sample application written and configured in 103 or 105?
If you create fresh configuration in 105 do you see any issues? (not sample app)
peter
I have the same issue, can anyone shed some light?