Hi,
We are using MC9S08GB60 Controller.I that i'm using IIC module for communication.Our's is POWER Domain project.In that we are using floating point variable for storing value of voltages like syst_vtg=58.90.
How can i change the data in syst_vtg of the power plant (which use the MC9S08GB60 controller ) from the remote side (which also using another MC9S08GB60 controller) through IIC. Can u suggest me how to write data to floating point variable and also how to read the data from floating point variable through IIC. And also i want to know the exact format in which HCS08 family IIC module works,because they gave IIC format like below,but they didn't mentioned the address of memory where we have to write.
start slaveaddress r/w data stop
But in other memory and all they clearly mentioned where to write (address register)as shown in below.
start slaveaddress r/w address register data stop;
Suggest me on this issue and attach example code if u have other than the code which is given in freescale data sheets.
With regards
Santhosh
Added p/n to subject.
Message Edited by NLFSJ on 2008-12-24 07:20 AM