i used imx6q sabreauto.
root@imx6qsabreauto# gst-inspect-1.0 ximagesrc
No such element or plugin 'ximagesrc'
I yocto build
conf/local.conf
IMAGE_INSTALL_append = " gstreamer1.0 "
IMAGE_INSTALL_append = " gstreamer1.0-plugins-base "
IMAGE_INSTALL_append = " gstreamer1.0-plugins-bad "
IMAGE_INSTALL_append = " gstreamer1.0-plugins-good "
IMAGE_INSTALL_append = " qtbase "
IMAGE_INSTALL_append = " qtdeclarative "
IMAGE_INSTALL_append = " imx-gpu-viv "
IMAGE_INSTALL_append = " libffi "
IMAGE_INSTALL_append = " gstreamer1.0-plugins-imx "
IMAGE_INSTALL_append = " gstreamer1.0-libav"
PACKAGECONFIG_append_pn-qtmultimedia = " gstreamer alsa openal"
PACKAGECONFIG_remove_pn-qtmultimedia = " pulseaudio"
PACKAGECONFIG_append_pn-gstreamer1.0-plugins-ugly = "a52dec lame mad mpeg2dec x264"
LICENSE_FLAGS_WHITELIST = "commercial"
bitbake fsl-image-qt5-validation-imx
Is there missing syntax?
Or was "bitbake" wrong?
regards.
I was thinking whether it's possible to harness the hardware codec for this purpose, so after playing around with GStreamer liteblue
Hello K Ms,
The conf file looks okay. Did bitbake finish without any errors?
The ximagesrc should be available along the gstreamer packages. Have you tried using it to see if it generates an error? You could test taking a screenshot with the command:
gst-launch-1.0 ximagesrc num-buffers=1 ! pngenc ! filesink location=./file.png
If it shows an error. Could you provide details on it?
Regards,
Thank you for answer.
root@imx6qsabreauto:~# gst-launch-1.0 ximagesrc num-buffers=1 ! pngenc ! filesink location=./file.png
WARNING: erroneous pipeline: no element "ximagesrc"
I can not find imagesrc.
bitbake was successfully build.
I can not find the libgstximgesrc file in the file system.
bitbake Wrong way?
regards
Thank you for answer.
root@imx6qsabreauto:~# gst-launch-1.0 ximagesrc num-buffers=1 ! pngenc ! filesink location=./file.png
WARNING: erroneous pipeline: no element "ximagesrc"
I can not find imagesrc.
bitbake was successfully build.
I can not find the libgstximgesrc file in the file system.
bitbake Wrong way?
regards
Thank you for answer. root@imx6qsabreauto:~# gst-launch-1.0 ximagesrc num-buffers=1 ! pngenc ! filesink location=./file.png WARNING: erroneous pipeline: no element "ximagesrc" I can not find imagesrc. bitbake was successfully build. I can not find the libgstximgesrc file in the file system. bitbake Wrong way? regards