imx6ul with 10.1 LVDS inch display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul with 10.1 LVDS inch display

1,523 Views
sarathak
Contributor I

Dear All,

I am new to BSP development in ,@imx6ul som. 

We are planning to use 10.1 inch LVDS display in I.MX6-UL based SOM,  

Please suggest me its is possible or not, If possible how to do this, 

Kindly help us.

0 Kudos
2 Replies

1,060 Views
embedded_Dev
Contributor III

Hello sarathak,

Can you please share the dtsi file for reference. I am using 7 inch LVDS LCD but i cant able to see anything on the screen. Can you please share ASAP.

Thank You

0 Kudos

1,174 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sarath

lvds lcds are not natively supported by i.MX6UL (there is no LDB module),

one can use some converter (parallel to lvds output) like DS90C385AMT or similar.

Note, also one will have to develop driver for it. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos