MPC57xx Motherboard 5V SR Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC57xx Motherboard 5V SR Problem

479 Views
lukezhang
Contributor III

Hi all,

I'm using MPC5777C 512DS with MPC57XX motherboard (SCH-27237 REV C) for my project. I found a very strange problem and don't know why it happen. The project involves an EEPROM external chip, MCAN module, RS232 module etc. My external EEPROM chip needs 3 pins to connect to 5V, so I decided to use 5V SR line supplying it. There're total 4 5V SR outputs on the top-right corner of the motherboard. Then I found:

   1. If I connect 3 of the 5V SR output to that 3 pins on the external chip straightly, my external chip works fine but the MCAN module doesn't work, sometimes RS232 module doesn't work as well.

   2. If I connect 1 of the 5V SR output to a breadboard power line, and from the breadboard power line, I connect 3 output to the external chip, my external chip and all other module work fine.

Since all 5V SR has the same effect (they pass the continuity checking), I'm wondering why the first case will cause other module not working. 

Regards,

Luke

0 Kudos
1 Reply

389 Views
lukezhang
Contributor III

For this problem, I have another finding, please refer to this problem MPC5777C MCAN Module Problem

Thanks

0 Kudos