Is there any documentation available for USB over-current detection in i.MX6ul?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any documentation available for USB over-current detection in i.MX6ul?

434 Views
hardikbehere
Contributor I

Hi,

In our application, we are using over-current detection to control Vbus supply using Vbus enable pin.

But after detection of  USB over-current signal, processer assert a low signal to Vbus enable pin and remains low though USB device is removed from the device, we require to reboot the device to work USB again.

Regards,

Hardik Behere

Labels (1)
0 Kudos
1 Reply

350 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hardik

over-current one can check PP bit USB_nPORTSC1 description

in sect.54.6.31 Port Status & Control (USB_nPORTSC1) i.MX6UL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos