Hi NXP Community,
I have to start a project with the iMX 8M EVK and I would like to know which peripherals are already enabled on the Android prebuilt images.
I need at least
Ethernet and WiFi connectivity
Audio output
Microphone
Camera
USB
Could you please help me?
Thanks in advance
Hi Massimiliano,
The prebuilt Android Demo Image for MCIMX8M-EVK could be downloaded from the following link:
O8.1.0_1.3.0_ANDROID_DEMO_8MQ_GA
In case of requiring specific drivers/features, you could build your own image using the source package from the following link:
O8.1.0_1.3.0_ANDROID_SOURCE_8MQ_GA
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Carlos,
thanks for your quick answer.
What I would like to know is the status of prebuilt image.
Does it enable the peripherals such as Ethernet, Audio output, microphone, Camera, USB or it enables only the display and the touch?
I need this info to try to estimate the effort needed to have the platform working.
Thanks in advance
Massimiliano
Hi Massimiliano,
Such details are included on the Release Notes of Android documentation package, available on the following link:
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------