VDDHIGH_IN supply for i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VDDHIGH_IN supply for i.MX6Q

1,315 Views
teikhooiteoh
Contributor I

Hi,

Does VDDHIGH_IN input supply for i.MX6Q required to be monotonic during rise time?

Any specifications on that?

In my design, VDDHIGH_IN is supplied by PMIC MMPF0100ANES VGEN5 (2.8V).

With just connection to the i.MX6Q input supply, a dip during the VDDHIGH_IN is observed.

pastedImage_1.png

Is this expected behavior?

Labels (2)
Tags (2)
0 Kudos
4 Replies

1,088 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

Doing a little further investigation, I found that the dip you are seen appears in the very beginning of the voltage power-on ramp-up curve, so it affects neither the power-up sequence nor further device operation.

 

You can find more details in the following link: https://community.nxp.com/message/805891


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,087 Views
teikhooiteoh
Contributor I

Hi Jose,

Is there any possible reason for this? VDDHIGH_IN only connected almost

directly from PMIC VGEN5 output to i.MX6 input.

I did observed that if measure on the VCC_VG5_2V8 output alone (isolating

by removing R706), there is no such dip during rising.

Regards,

TEOH TEIK HOOI 张泽晖 | Staff Engineer | Electrical Engineering, Medical

R&D Division | Olympus Singapore Pte Ltd

Phone: (65) 6777 8978 | DID: (65) 6870 2585 | Mobile:(65) 9459 7235 | Fax:

(65) 6870 2508 | Email: teikhooi.teoh@olympus-ap.com

0 Kudos

1,088 Views
reyes
NXP TechSupport
NXP TechSupport

Hi TEOH TEIK HOOI,

 

The dip is caused by a current demand during the power-up sequence that VGEN5 cannot provide.

 

VDDHIGH was placed on VGEN5 early in the design as a compromise solution for a board designed primarily for software development. Validation of the i.MX6 processor has shown that operations at elevated temperatures may cause VDDHIGH_IN to require much more current than VGEN5 can supply. It is recommended for robust designs potentially operating at more extreme temperatures for VDDHIGH to be supplied from a power rail that can supply 250 mA or more.

This allows for datasheet maximum of 125 mA for internal VDDHIGH_IN loads plus 125 mA for external PHY IO loads.

 

Check Page 20 of the i.MX6Quad SABRE reference design that you can download from the following link: https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/sabre-development-...

 

In the i.MX6Quad SABRE design, you will find an optional LDO (U9) that could be reconfigured to supply both VDDHIGH_IN and VDD_SNVS_IN loads to meet the additional current requirements.

 

Thanks,

Jose

0 Kudos

1,088 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

According to the Hardware development guide for i.MX 6Q, VDDHIGH_IN should be the second in the power-up sequence and is typically supplied by SW2 of the PMIC: https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

 

Probably this behavior is caused due to the sequence used in your application.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos