MIMXRT1050-EVK "bricked" with no debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1050-EVK "bricked" with no debugger

381 Views
j5504139
Contributor I

I've accidentally flashed the m4  (M20AGV) based debugger/programmer on my MIMXRT 1050-EVK board, by connecting to the mini JTAG (DOH). It seems that with invalid flash on that chip, the M7 won't even boot.

Is the binary for the CMSIS-DAP for the M4 available somewhere?

Is it otherwise somehow possible to "unplug" the m4 and have the m7 working without it?

0 Kudos
1 Reply

300 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Martin,

You could try reprogramming the bootloader  (with external debugger) and/or the firmware application according with the instructions from the following link:

https://www.nxp.com/support/developer-resources/run-time-software/kinetis-developer-resources/ides-f...


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos