AnsweredAssumed Answered

NFC SNEP with NT3H2111

Question asked by Sean Lanigan on Nov 18, 2018
Latest reply on Feb 1, 2019 by Erich Reisenhofer

Hi there,

 

We're working on a product using the NT3H2111 - so far we have used it with success writing NDEF messages via I²C into the EEPROM and then reading them back from an Android phone, and vice-versa.

 

Now we are looking to implement something more advanced, and I have come across NXP's "NFC Reader Library", which claims to support SNEP (and other features).

 

The NT3H2111 is not listed as supported by this library, is there any other similar library which could create a SNEP target with an NT3H2111? The chip has "passthrough" mode, is there a library which can use this in a standard way which would not necessarily require a custom Android application?

Outcomes