Hello all, i tested MFG Tool in Ubuntu 16.04 with i.MX8MQuad Evaluation Kit (using the provided scripts) but i could not load an image because of error code #24. The log message shows 'Invalid device name MX8QM' but according to 'ucl2.xml' (PID, VID and 'lsusb' command) i should get the configuration for MX8MQ.
'ucl2.xml' configuration tags:
<CFG>
<STATE name="BootStrap" dev="MX8QM" vid="1FC9" pid="0129"/>
<STATE name="BootStrap" dev="MX8QXP" vid="1FC9" pid="012F"/>
<STATE name="BootStrap" dev="MX8MQ" vid="1FC9" pid="012B"/>
<STATE name="Updater" dev="MSC" vid="066F" pid="37FF"/>
</CFG>
I also changed the 'cfg.ini' file but i got the same error.
The same files worked without problems in Windows 8.
What is wrong?
Am i missing something in Linux?