about X11 on 4.9.88-2.0.0-ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about X11 on 4.9.88-2.0.0-ga

Jump to solution
858 Views
MasakiHayakawa
Contributor III
Hi,
BSP:4.9.88-2.0.0 ga
SOC:i.MX6QP
We created yocto filesystem using the following DISTO setting.
DISTRO=fsl-imx-x11 MACHINE=imx6qpsabresd
Please refer to attached file, this file is included in BSP folder.
The following description is about i.MX8 ?
x11         X11  (not supported in 4.9.88-2.0.0 ga release)
Becase we found the following descrition on i.MX_Yocto_Project_User's_Guide.pdf
fsl-imx-x11 - X11 graphics are not supported on i.MX 8.
Best Regards.
Labels (2)
0 Kudos
1 Solution
527 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Masaki Hayakawa,

X11 is not supported for the i.MX8 processors on this BSP, but it is supported for i.MX6. The README is not clear on this, my apologies.

I hope this helps!

Regards,

View solution in original post

0 Kudos
1 Reply
528 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Masaki Hayakawa,

X11 is not supported for the i.MX8 processors on this BSP, but it is supported for i.MX6. The README is not clear on this, my apologies.

I hope this helps!

Regards,

0 Kudos