AnsweredAssumed Answered

I.MX6 SSI2 BCLK and LRCK configuration problem

Question asked by 嘉麟 王 on Nov 15, 2018
Latest reply on Nov 15, 2018 by igorpadykov

I use one sound card, configuration using SSI2, I2S as the master, AUD3 audio output, AUD4 Bluetooth, AUD5 MIC input. Now the problem is that AUD3 and AUD4 need to output 44.1K LRCK, AUD5 need to output 48K LRCK, after I change the LRCK, AUD3, AUD4, AUD5 LRCK change at the same time, and the clock is the same. Can I modify each AUD and output different LRCK at the same time?

Outcomes