AnsweredAssumed Answered

Generate binary artifact with LPCXpresso

Question asked by Alex Rebega on Nov 14, 2018
Latest reply on Nov 15, 2018 by soledad

Hello. I am using LPCXpresso to develop software for LPC11C12. 

The generated build-artifact has the .axf extension. I would like to generate a binary file from that so I am using the following command: 

arm-none-eabi-objcopy --reverse-bytes=4 -v -O binary "myArtifact.axf" "myArtifact.bin"

 

I am getting this error:

arm-none-eabi-objcopy.exe: cannot reverse bytes: length of section .debug_info must be evenly divisible by 4

 

A .bin file is generated but when I write it to the flash memory it does not work (it works when I write the axf file to flash). If I inspect the axf and bin files using a hex-editor the bytes order is reversed.

 

Can anyone suggest a solution, maybe a way to add a padding to debug_info to make it divisible by 4? I would prefer not to reverse the bytes order manually as I want to use the .bin file in production.

Outcomes