i.mx8m,3.3v改成1.8v相关问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx8m,3.3v改成1.8v相关问题

1,929 Views
aaron_zeng
Contributor II

你好:

客户正在设计IMX8M硬件原理图,有个问题请教一下:从官网上下载评估板原理图,想将下图3.3V供电-NVCC_3V3,改成1.8V供电。

1.png

供电1.8V电源采用官网推荐的MC34PF4210A1ES电源管理芯片的SW4通道,NVCC_1V8

 2.png

问题1:如果将NVCC_3V3改成NVCC_1V8后,boot 配置电路 BT_CFG  IO端口 上拉电阻的电源 NVCC_SNVSVNCC_JTAG_3V3VNCC_SAI1_3V3是否需要做相应的调整,以保证IO口的电平保持一致。

3.png

4.png

问题2:如果不改变boot 配置电路 调整imx8电源供电,VNCC_JTAG_VNCC_SAI1供电采用3.3V,其余采用1.8V,具体如下下图所示,是否可行?。

5.png

请帮忙解决一下,万分谢谢!

 

Labels (2)
0 Kudos
2 Replies

1,575 Views
aaron_zeng
Contributor II

thanks Wigros.

还有一个关于HDMI接口的问题:

           从评估板的原理图中可以看到,HDMI_DDC_SCL、HDMI_DDC_SDA、HDMI_HPD、HDMI_CEC都是从原理图中直接连到HDMI接插件上,HDMI_DDC_SCLHDMI_DDC_SDA上拉电阻+5v供电,HDMI_CEC上拉电阻+3.3v供电(如下入1,2),从手册中查到这些信号都采用HDMI_AVDDIO(1.8V)供电,即HDMI_DDC_SDA,HDMI_HPD,HDMI_CEC的IO口电平1.8V。但HDMI标准上,HDMI_HPD电平是5V,HDMI_DDC_SDA电平是5V,HDMI_DDC_SCL电平是5V,HDMI_CEC电平是3.3V。

问题:IO电平是不是存在电平不匹配,直接与外部显示器相连,会不会出问题?

1.png

2.png

3.png

0 Kudos

1,575 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello zeng,

See below, please!

--------------------------------

>>问题1:如果将NVCC_3V3改成NVCC_1V8后,boot 配置电路 和BT_CFG  IO端口 上拉电阻的电源 NVCC_SNVS、VNCC_JTAG_3V3、VNCC_SAI1_3V3是否需要做相应的调整,以保证IO口的电平保持一致。
(1)boot_mode1 & boot_mode0 pin's leve is determined by NVCC_JTAG. so if NVCC_JTAG is 1.8V, BOOT_MODE1 & BOOT_MODE0 pins should be 1.8V IO.
(2)SAI1's level is determined by NVCC_SAI1, BT_CFG  IO should be also 1.8V

>>问题2:如果不改变boot 配置电路 , 调整imx8电源供电,VNCC_JTAG_、VNCC_SAI1供电采用3.3V,其余采用1.8V,具体如下下图所示,是否可行?。
Yes, no porblem.  I think the way is better than above.

-------------------------------------

Have a nice day!

NXP TIC weidong sun

0 Kudos