AnsweredAssumed Answered

LS1043A and family transient response

Question asked by Abhinav Sharma on Nov 8, 2018
Latest reply on Nov 9, 2018 by andrei.skok

Hi,

 

I have a question pertaining more specifically to the 1043A as well as the other LS10XXA devices. The datasheet describes either +50mV/-30mV or +/-30mV on most 1.0V rails for the recommended values. My question specifically is: is this the total range or just the DC variation range. Is there another 30mV for transient variation effectively making this +80mV/-60mV and +/-60mV or is it strictly as described.

 

Thanks,

Abhinav.

Outcomes