Hi All,
I am evaluating the i.MX6SoloXSabreSD board and have my application software running on the SDK build. I need to interface to a 4-wire resistive touch chip, TSC2046. Has anyone used a 4-wire resistive touch? Can anyone point me to a driver that will work on the i.MX6SoloX?
I built a working u-boot/kernel/filesystem using fsl-yocto-L4.9.11_1.0.0. Any pointers would be greatly appreciated.
Thanks,
Larry
Hi Larry
for TSC2046 may be useful below
tsc2046 (/ads7846) on imx6 "no irq" problem
Tweaking Froyo for Nitrogen Part 1: touch support - Boundary Devices
Configuring i.MX6 boards for different screens - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------