How to use lwip project in MPC5748G?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use lwip project in MPC5748G?

805 Views
klimmmike123456
Contributor II

How to use lwip project in MPC5748G?
We use mpc5748g devkit , S32 Design Studio for Power Architecture Version 2017.R1 and S32DS lwip_mpc5748g project in example.

This project description contain have udp_echo and tcp_echo,but we use this software (can send tcp packet and udp packet http://sourceforge.net/projects/sockettest/ )to send the packet to the board without any return.

I also used the following setting :

I use the cable line to directly link the PC to the board.I set the PC_ip address is 192.168.0.201,the board_ip address is 192.168.0.200.The board_mac address is 10:11:12:00:00:00,and PC set the arp table.After completing these setting and send packet,but there is no any return.

Someone can tell me what happened?Or is this project not done this way,can anyone give me advice?

Labels (1)
1 Reply

588 Views
gangzhou
Contributor II

I have the same question.How to do?

0 Kudos