wake up from usb(i.MX6)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wake up from usb(i.MX6)

962 Views
hyunhoshin
Contributor III

I want to use USB type LTE Dongle on i.MX6

I wonder if i.MX6 can wake up via USB LTE modem when it is in sleep mode.

Labels (1)
Tags (3)
0 Kudos
1 Reply

747 Views
igorpadykov
NXP Employee
NXP Employee

Hi hyunho

yes i.MX6 can wake up via USB, for usage one can follow sect.39.2.4 USB Wakeup Usage

attached Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos