AnsweredAssumed Answered

RAM limits for various i.mx6 devices

Question asked by David Luberger on Nov 1, 2018
Latest reply on Feb 28, 2019 by David Luberger

Why isn't the max RAM listed on the product pages for the processors? I have to dig into each separate reference manual and even then it isn't clear from the memory map whether the value i'm looking at is the actual max RAM size.

Is there a table or chart somewhere that lists the max DDR size for each processor? I learned too late after designing my imx6ul board with an 8Gb DDR3L IC that that processor would only use up to 512MB which is too low for what I need.  I need to be able to compare each processor by types of video peripherals available (parallel LCD, LVDS, HDMI), max speed (I need 1GHz), and max RAM (as I said, I need at least 1GB but I want to know the max I can use) in order to make a better decision about which processor i should go with.

Outcomes