AnsweredAssumed Answered

Current sinking capability of iMX7 GPIOs when configured as Open Drain outputs

Question asked by Deepak Kukreja on Nov 1, 2018
Latest reply on Nov 1, 2018 by igorpadykov

Hi,

 

I was trying to find the current sinking abillity of GPIO pins of the iM7D SoC when configured as open drain output.

 

I could find the current sinking/sourcing capability for Push/Pull outputs but not for open drain outputs in the iMX7 datasheet:

 

A peripheral pin would be driving a CMOS Chip that is biased (supply voltage is at 5V). So I was thinking if it is possible to configure this pin(iMX7) as open drain and pull it up through a resistor to 5V to interface these devices.

Outcomes