AnsweredAssumed Answered

I want to use the JFFS2 file system in the QSPI Flash of the LS1012A.

Question asked by 인섭 심 on Oct 31, 2018
Latest reply on Oct 31, 2018 by 인섭 심

Looking at kernel.its

 

    images {
        kernel@1 {
            description = "ARM64 Linux kernel";
            data = /incbin/("./arch/arm64/boot/Image");
            type = "kernel";
            arch = "arm64";
            os = "linux";
            compression = "none";
            load = <0x80080000>;
            entry = <0x80080000>;
        };
        fdt@1 {
            description = "Flattened Device Tree blob";
            data = /incbin/("./arch/arm64/boot/dts/freescale/fsl-ls1012a-frdm.dtb");
            type = "flat_dt";
            arch = "arm64";
            compression = "none";
            load = <0x90000000>;
        };
        ramdisk@1 {
            description = "LS2 Ramdisk";
                        data = /incbin/("./ramdisk.ext2.gz");
            type = "ramdisk";
            arch = "arm64";
            os = "linux";
            compression = "none";
        };
    };

 

 

I want to add JFFS2 File System here. Is it possible?

If so, how do I set it up?

Outcomes