FS32K MPU using MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS32K MPU using MCUXpresso IDE

1,586 Views
huang_hw
Contributor II
I am trying to develop using FS32K MPU (FS32K148UJT0VLQT). The development tool that is recommended on NXP web-site is "S32 Design Studio IDE for Arm® based MCUs".

Since this is a new project, I thought the IDE "MCUXpresso IDE" should be used as this is the new IDE that NXP will support and develop.

Question: For a new project using FS32K148, should the "MUXpresso IDE" or "S32 Design Studio IDE for Arm based MCUs' be used?

Thanks.

Tags (2)
0 Kudos
1 Reply

1,024 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

For S32K1xx devices please use S32 Design Studio IDE for Arm. This is the tool designed for S32K1xx devices, so it provides an better integrations with gdb, debuggers etc. Also, SDK is compatible just with Design Studio.

Probably with extra effort you can start your project in MCUXpresso IDE, but it is targeted for Kinetis devices.

Best regards,

Razvan