AnsweredAssumed Answered

I2C communication with Honeywell HumidIcon RH sensor problem

Question asked by yinni@qubitsystems.com on Oct 29, 2018

Hello,

I used Sensirion SHT35 for humidity and temperature measurement and the I2C communication between my Kinetis K50 100MHz 100LQFP and the sensor has been working fine. Now we switched to Honeywell Humidlcon RH sensor. When I sent out the measurement request command (which is very simple, just the 7-bit sensor address, 0x27 by default, followed by a '0' as write), the sensor never returned ACK.

 

I first check the hardware connection, which is strictly conformed with the sensor datasheet, measured the power supply voltage, which is 3.3V as expected, and reduced the SCL frequency to be lower than 100kHz, still no ACK from the sensor.

 

I suspected the sensor was damaged during soldering, and replaced it with a new one, the same result. I am on my wits' end, any suggestion would be appreciated.

 

Please find the attached for the waveform from logic analyzer and part of the code.

Attachments

Outcomes