Hi I download the IR remote controller/ receiver example form the following website.
I downloaded Keil version 5 to run the project which is version 4 project. Hence I downloaded the legacy support in order to open version 4 project in Keil as shown in the attached picture.
I think there should be more c and h files instead of just files related to GPIO. Like lpc8xx_mrt.c, lpc8xx_uart.c, lpc8xx_sct.c etc.
Could you help me on this? Thank you very much!
Hello Chen yi,
No, the project is correct, no files is missing.
If you check the AN11511_1.pdf, you will also find it is correct, please check this block diagram:
It use the SCT, gpio to realized it.
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------