* Environment : JN5169, JN-SW-4168, Coordinator, RF Channel(11,14,15,19,20,24)
When the coordinator started with ZPS_eAplZdoStartStack () in some circumstances , It meets stack event ZPS_EVENT_NWK_FAILED_TO_START.
That circumstances is several WiFi routers around.
If I turned off several WiFi routers around, ZPS_EVENT_NWK_STARTED is generated.
Is there a good solution without turning off the WiFi router around?
Hi Lee,
I suggest you to switch you application to channels where is not overlapped with typical Wi-Fi spectrum. Hopefully, this will make your network can co-exists even though you have several Wi-Fi routers around.
802.15.4 open channels when Wi-Fi fully utilized the band: 15, 20, 25 and 26.
I hope this helps.
Best regards,
Felipe
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Felipe,
I have tested but that channel is sometimes occurs event ZPS_EVENT_NWK_FAILED_TO_START.
Is it possible to set the channel manually if an event occurs ZPS_EVENT_NWK_FAILED_TO_START?
Best regards,
Lee
Hi Lee,
Yes, it is possible to change your network channel. You can configure that in bdb_options.h.
Best regards,
Felipe
Hi Felipe,
Where is bdb_options.h?
I am using JN-SW-4168-SDK - JN516x ZigBee Home Automation SDK.
Hi Lee,
In Home Automation SDK you can look in JN-AN-1184 Router example. Using that AN you can change the channel in app_router.c file and vStartup function.
What AN are you using?
Best regards,
Felipe
Hi Felipe,
I am using JN-AN-1189 example.
And I will test with vStartup function source of JN-AN-1184 Router example.
Thanks.
Hi Felipe,
Thank you for your kindly reply.
It is now completed about my question.
Best regards,
Felipe