link application to ram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

link application to ram

1,543 Views
rans
Senior Contributor I

Hello,

Is it that the "link application to ram" idea is that we can easily start debug application which usually runs in flash ?

Isn't it possible to debug application in flash ?

Thank you,

ranran

3 Replies

1,230 Views
converse
Senior Contributor V

Yes, you can debug in flash. This is how most people develop their applications. The link-to-ram is a specialist setting that you do not need to use.

1,230 Views
rans
Senior Contributor I

Thanks,

Just for my general knowledge, what was the idea behind "link to ram" ? Is it for flash that can be debugged ?

Thanks,

ranran

0 Kudos

1,230 Views
BlackNight
NXP Employee
NXP Employee

It is for running your application in RAM instead of FLASH. That was necessary in 'old' days if you only were able to program the FLASH a few time until it weared out. Another benefit is that on some targets running the application in RAM is faster, but in that case you probably want to have the code in FLASH and then copy it to RAM at runtime.

I hope this helps,

Erich

0 Kudos