Dear team,
My customer is trying to re-new their i.MX257 custom board. And they have a question about the external capacitor which should connect to NVCC_DRYICE.
Now they are using a ceramic capacitor for the external capacitor.
For general, a ceramic capacitor has a DC-Bias-Characteristic which the capacitance can decrease.
On your datasheet, it is said that “An external capacitor no less than 4 μF must be connected to NVCC_DRYICE.”.
Could you show me whether one has to consider also the capacitance decrease when selecting the capacitor?
Thanks,
Miyamoto
Hi Miyamoto
>whether one has to consider also the capacitance decrease when selecting the capacitor?
yes this also should be taken into account, 4 μF min. value should be followed in all operating conditions.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------